Hello all.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hello all.

1,874 Views
prasadrao
Contributor I

Im working with k70 and using can im trying to communicate with bust master.

The function FLEXCAN_RX_Messages not able to read messages which are send by the bus master.

0 Kudos
Reply
2 Replies

1,760 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Please check attached TWR-K70F120M board FlexCAN RX demo with CodeWarrior Processor Expert software.


Wish it helps.
best regards
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,760 Views
prasadrao
Contributor I

Thanks for your replay...

But I written code for can protocol using MQX.

I can communicate with the busmaster.

The function FLEXCAN_Rx_message returning the value is no messages in the buffer.

i am waiting for replay.

Thanks and Regards

Prasad

0 Kudos
Reply