Hello Sir, Actually we worked first for MK60DN512VLQ100 IC for Ethernet communication. We used keil uv5 for the development. Sample generated code was taken from code warrior(10.1) and implemented in our keil version. With this we are ab

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hello Sir, Actually we worked first for MK60DN512VLQ100 IC for Ethernet communication. We used keil uv5 for the development. Sample generated code was taken from code warrior(10.1) and implemented in our keil version. With this we are ab

1,172件の閲覧回数
leninprabhakar
Contributor I
              Actually we worked first for MK60DN512VLQ100 IC for Ethernet communication. We used keil uv5 for the development. Sample generated code was taken from code  warrior(10.1) and implemented in our keil version. With this we are able to transmit and receive data through Ethernet.
             Coming to MK66FN2M0VLQ18 we have created one more project in keil and the code we copied from  MK60DN512VLQ100 and trying to send the data. In this present IC transmit interrupt is not occurring and the data we are unable to send through Ethernet module.
            Please suggest us what could be the problem and if any generated code or source code available in keil for Ethernet communication forward us
タグ(3)
0 件の賞賛
返信
1 返信

1,101件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

NXP provides KSDK V2.0 software for Kinetis K66 product, which includes lwip TCP/IP stack and related demo example.

Please download KSDK V2.0 software from here.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信