Have you any reference code for RAM test of external DDR2 on the K70 kinetis

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Have you any reference code for RAM test of external DDR2 on the K70 kinetis

1,681 Views
poul-erikhansen
Contributor II

I am worried that any error must be hidden by a catch function.


Poul-Erik.



Labels (1)
0 Kudos
Reply
1 Reply

1,402 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please refer attached SRAM memory test code for internal SRAM, which is also suitable with DDR2 memory test.

About K70 DDR2 memory controller setting, please download KINETIS_K70_DDR_INIT (Kinetis K70 DDR memory initialization tool) from below link:

K70_120: Kinetis K70 Graphic LCD 120/150 MHz MCUs
Wish it help.

best regards,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------