Has anyone tried to emulate CEC(Consumer Electronics Control) using GPIO?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Has anyone tried to emulate CEC(Consumer Electronics Control) using GPIO?

2,859 Views
koichimatsuo
NXP Employee
NXP Employee

About HDMI CEC

High-Definition Media Interface (HDMI) incorporates a single-wire interface called Consumer Electronics

Control (CEC) in order to support 'one touch' control features in newer audio/visual systems.

CEC is not a conventional bus and is not readily found on microcontrollers like the more common protocols I2C or SPI.

Currently TI is emulating this interface using GPIO.

Has anyone tried to emulate this interface using GPIO?

http://www.ti.com/lit/an/slaa377/slaa377.pdf


Regards,

Koichi

Tags (1)
0 Kudos
Reply
3 Replies

2,277 Views
chetkaufman
NXP Employee
NXP Employee

I have a customer who also wants to control CEC line using a MCU GPIO line.    Can I have access to the answer that was provided to Koichi Matsuo?

0 Kudos
Reply

2,277 Views
karina_valencia
NXP Apps Support
NXP Apps Support

michaelsteffenfae​  can you help Chester?

0 Kudos
Reply

2,277 Views
karina_valencia
NXP Apps Support
NXP Apps Support

HI Koichi,

follow up will be provided in your internal post. I will close this  one.