Glucometer project!?!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Glucometer project!?!

4,576 Views
shahrzadshahria
Contributor II

Hi everyone

I'm working on glucose meter project and Im not sure wat component I should use

based on my research i need opamps, triamps, ADC, DAC .. but isnt Kinetis K50 or K53 includes them all?
and wat can i use instead of K50?

8 Replies

4,340 Views
albertovargas
NXP Employee
NXP Employee

Hi Shahrzad,

K50 Family is suited for medical applications. Here is the K50 Family block diagram; as you can see the analog part has ADC, DAC, OPAMP and TRIAMP

K50_BD.jpg

And here is the Glucose Meter Fundamentals and Design AppNote: http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4364.pdf?fpsp=1&WT_TYPE=Application...

Best Regards,

Alberto

0 Kudos
Reply

4,340 Views
shahrzadshahria
Contributor II

well thank you both Ping and Alberto

but I don't have any access to K50 and I'm looking for cheaper MUC that

suited for my project

On Tue, Sep 24, 2013 at 10:31 PM, Alberto Vargas Rodriguez <

0 Kudos
Reply

4,340 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Shahriari,

I'm glad to see your reply and I think it must has some MCU could meet your requirement from Freescale. So you can choose the MCU which you want by the help of Solution Advisor and the link is below.

http://freescale.transim.com/solutionadvisor/LandingPage.aspx

Regards,

Ping

4,340 Views
shahrzadshahria
Contributor II

Thank you Ping

you were so helpful

4,340 Views
jeremyzhou
NXP Employee
NXP Employee

You're welcome.

4,340 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Shahriari,

I think the Kinetis K50 series can meet your requirements. Attached is K50 Family Product Brief which provide a lot information of K50 series and you can browse it.

Freescale also provide Glucose Monitor application based on K50 for customer.

First link is about Continuous Glucose Monitor and the second is about Pulse Oximeter Fundamentals and Design

Consumer Continuous Glucose Monitor Solutions By Freescale

http://cache.freescale.com/files/32bit/doc/app_note/AN4327.pdf?fpsp=1&WT_TYPE=Application%20Notes&WT...

Regards,

Ping

4,340 Views
shahrzadshahria
Contributor II

Is there any other MUC that I can use instead of the Kinetis series?

0 Kudos
Reply

4,340 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Shahriari,

Does not the K50 series MCU meet your requirement? If not, you can choose K60 or K70 as replacement.

The K50 MCU family provides designers with an analog measurement engine consisting of

integrated operational and transimpedance amplifiers as well as high-resolution ADC and DAC

modules and is very suitable for medical measurement.

Regards,

Ping

0 Kudos
Reply