Flexcan stall status

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Flexcan stall status

1,101 次查看
LArmstrong1985
Contributor III

Hi,

I am using the FlexCAN on the FRDM-K64 demo board starting from the example.

It happened several times that the internal controller stall on TxBusy status and I am no longer able to send any packets. How should this situation be managed and restore the correct functioning of the CAN controller inside the micro? In the example the callback only manages the RxIdle and TxIdle states.

Thank you very much!

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,028 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello Fabio Benevento

The TxBusy can be caused because the Tx is not being listened. It could be helpful if you detail me the value of the CANx_ESR1 register.

Also, make sure that the loopback mode is active, the ID from Rx and Tx needs to match.

 

Let me know if this is helpful, if you have more questions do not hesitate to ask me.

Best regards,

Omar

0 项奖励
回复