Flashing FRDM-KW36 board with a .bin file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flashing FRDM-KW36 board with a .bin file

1,734件の閲覧回数
michaelestrin
Contributor I

Hi,

I've a .bin file I've compiled with IAR. Is there any simple way to flash it to a FRMD-KW36 board?

The IAR has a built-in flashing functionality to download images, but it only supports debug .out ELF files. 

Thanks!

Michael

ラベル(1)
0 件の賞賛
返信
1 返信

1,406件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Michael,

    Please check your FRDM-KW36, it should have the on board debugger, if you can firmware the on board debugger with JLINK firmware, then you can use the JLINK software to download the .bin file directly.

 Eg, you can use the JLink command, with commander: loadfile xxx.bin

to download the code.

 The FRDM-KW36 JLINK firmware can be downloaded from this link:

https://www.segger.com/downloads/jlink/46_OpenSDA_FRDM-KW36 

    You need to make the FRDM board enter debugger mode, then send the above jlink firmware to the bootloader, after power on again, you on board will be changed to the JLINK firmware.

   But at first, you need to install the JLINK software, which can be download from this link:

https://www.segger.com/downloads/jlink/JLink_Windows.exe

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信