Flash program using one mcu to another usign opensda

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash program using one mcu to another usign opensda

1,696 Views
sunilkumar_sing
Contributor III

Hi,

I have three frdm board two KL25 and one KL26 and I need to program my prototype board which is  based on kl26(256KB).

I have successfully program KL25 to KL25 but no luck on KL26.

I follow the below link:

http://mcuoneclipse.com/2013/04/21/using-the-freedom-board-as-jtag-programmer

How can I program my prototype board which is based on (MKL26Z256VLH4,MKL25Z128VFM4) using frdm kl26,kl25.

Please reply as soon as possible, Its urgent for me.

Let me know if more information required.

Thanks,

Sunil

,

0 Kudos
Reply
1 Reply

1,593 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Sunil,

It failed to program the KL26 by using the FRDM-KL26 board, however the FRDM-KL25 did it.

The flow of the thread "Using the Freedom Board as SWD Programmer" definitely is correct, I also did it by following the steps.

So I'd like to suggest that you should check the hardware of the prototype KL26 board at first, and I'm going to share another thread to you.

I think this thread can provide another approach to fix the issue and the link as below.

Using the Freescale Freedom (FRDM-KL43Z) to Debug other Boards | MCU on Eclipse
Have a great day,

Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply