Flash program using one mcu to another usign opensda

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash program using one mcu to another usign opensda

1,700件の閲覧回数
sunilkumar_sing
Contributor III

Hi,

I have three frdm board two KL25 and one KL26 and I need to program my prototype board which is  based on kl26(256KB).

I have successfully program KL25 to KL25 but no luck on KL26.

I follow the below link:

http://mcuoneclipse.com/2013/04/21/using-the-freedom-board-as-jtag-programmer

How can I program my prototype board which is based on (MKL26Z256VLH4,MKL25Z128VFM4) using frdm kl26,kl25.

Please reply as soon as possible, Its urgent for me.

Let me know if more information required.

Thanks,

Sunil

,

0 件の賞賛
返信
1 返信

1,597件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Sunil,

It failed to program the KL26 by using the FRDM-KL26 board, however the FRDM-KL25 did it.

The flow of the thread "Using the Freedom Board as SWD Programmer" definitely is correct, I also did it by following the steps.

So I'd like to suggest that you should check the hardware of the prototype KL26 board at first, and I'm going to share another thread to you.

I think this thread can provide another approach to fix the issue and the link as below.

Using the Freescale Freedom (FRDM-KL43Z) to Debug other Boards | MCU on Eclipse
Have a great day,

Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信