Flash Life Cycle

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash Life Cycle

2,183 Views
davidzhou
Contributor V

Hi,

I have K60 tower board with 1M flash memory.

My question is general flash writing life cycle. I have hard time to find.

Is about 10,000,000?

What is best solution if I need to save run-time data in to non-volatile memory every second? EEPROM / Flash?

Thank you,

David Zhou

0 Kudos
Reply
1 Reply

1,912 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello David Zhou:

That information is available in the Kinetis device datasheet. See the picture below from the MK60FN1M0VLQ12 datasheet:

Flash_endurance.jpg

Now for your particular case you need to save data very often (1 sec), so maybe an external EEPROM is a better option.

I hope this helps.


Best Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply