Fatal error:Reading CPU status failed Session aborted with IAR and I-Jet

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fatal error:Reading CPU status failed Session aborted with IAR and I-Jet

4,280 Views
thaohm2
Contributor I

I am runnign the Demo and example applications are provided by NXP to demonstrate peripheral drivers, FreeRTOS kernel usage and to highlight the main features of the i.MX7Dual SABRE board.

0.png

I have tried to download Image which compiled successfully using I-Jet Debugger, but the error occurred.

1.png

Below is the detailed log:

IAR Embedded Workbench 8.32.3 (C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.2\arm\bin\armproc.dll)
Loaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.2\arm\config\debugger\NXP\iMX7_M4.dmac
Loaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.2\arm\config\debugger\NXP\iMX7_Trace.dmac
Loaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.2\arm\config\debugger\NXP\iMX7_Common.dmac
Loading the I-jet/JTAGjet driver
Probe: Probe SW module ver 1.61
Probe: Option: trace(Auto,size_limit=100%)
Probe: Found I-jet, SN=90275
Probe: Opened connection to I-jet:90275
Probe: USB connection verified (8115 packets/sec)
Probe: I-jet, FW ver 7.2, HW Ver:B
Probe: None or IJET-MIPI10 adapter detected
Probe: Versions: JTAG=1.84 SWO=1.40 A2D=1.71 Stream=1.50 SigCom=2.44
IMX7 device specific processor status testing in use.
Emulation layer version 4.46
JTAG clock detected: 12MHz
JTAG chain "TDI->TAP#0[Cortex:IR=4]->TDO" verified.
Notification to core-connect hookup.
CPU status FAILED
Connected device does not match requested core Cortex-M4.CoreSight error : Firmware scan error (may indicate pending fault AP transaction that must be aborted).
MultiCore: Asynchronous core execution FORCED.
MultiCore: Synchronous core execution DISABLED.
LowLevelReset(hardware, delay 200)
Connecting to TAP#0 DAP AHB-AP-CM port 4 (IDR=0x24770011).
Recognized CPUID=0x410fc241 Cortex-M4 r0p1 arch ARMv7-M
Debug resources: 6 instruction comparators, 4 data watchpoints.
Notification to init-after-hw-reset hookup.
Connecting to TAP#0 DAP AHB-AP-CM port 4 (IDR=0x24770011).
Recognized CPUID=0x410fc241 Cortex-M4 r0p1 arch ARMv7-M
Debug resources: 6 instruction comparators, 4 data watchpoints.
CPU status - IN RESET
CPU status - IN RESET
Fatal error: Reading CPU status failed Session aborted!
IAR Embedded Workbench 8.32.3 (C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.2\arm\bin\armproc.dll)
Loading the I-jet/JTAGjet driver

Is anybody able to help me out ?

Thanks a lot. 

0 Kudos
Reply
1 Reply

4,167 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Thao M. Hoang,

  Do you use i.MX7Dual SABRE board, right?

  If yes, please create a new question post in the I.MX community, this community is the kinetis MCU community.

  i.MX Processors 

  Please create the new question post in the I.MX processors area.

  Wish it helps you!

Wish it helps you!

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply