FTM jitter compared to TPM in Kinetis devices

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FTM jitter compared to TPM in Kinetis devices

1,380件の閲覧回数
ejohnson
Contributor I

Hello, I am considering using a Kinetis device with the FTM peripheral in an application that has very tight requirements on jitter for certain signals. We had previously discovered that the TPM on Kinetis devices had sufficiently low jitter to meet our application's requirements; however, the ambient temperature ratings were too low. The Kinetis EA family meets our ambient temperature requirements but trades the TPM peripheral for the FTM. Does the FTM have similar jitter to the TPM?

Thanks!

0 件の賞賛
返信
1 返信

1,215件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Erik,

You can treat the FTM as an advanced TPM, in another word, the FTM is built upon the TPM.

So I think they have similar property specifications.

Hope this helps!
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信