FRDM-Kx boards not in processor expert

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-Kx boards not in processor expert

1,476件の閲覧回数
kevinangus
Contributor III

While having to go back to the drawing board for a 'lower' cost solution I looked at the KE0x and KL0x lines, I found support for the processors in Process Expert but the 'Board' support was not there:

FRDM-KE02Z40M

FRDM-KE02Z

FRDM-KL02Z

FRDM-KL03Z

FDRM-KL46Z

FRDM-K64F

I have the KL46Z and K64F but those are not supported in PE.

Any idea when the FRDM boards will be supported in PE?

The MKL02Z16VFK4 is high on my list as well as the MKL03Z16VFG4.

Thanks

0 件の賞賛
返信
1 返信

1,246件の閲覧回数
santiago_gonzal
NXP Employee
NXP Employee

Hello Kevin,

The only support for boards that Processor Expert adds is that it creates some components already configured for the boards.

For example, for the FRDM-KL25 there is a Red_LED component, that is basically a GPIO component with a custom name and the pin already configured to the one that is connected to the red pin of the RGB Led in the board.

But all the microcontrollers used in the boards you mention are already supported in Processor Expert, so you can begin to work with all the boards immediately.

Regards,


Santiago

0 件の賞賛
返信