FRDM-KL26Z eval board, openSDA not working.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-KL26Z eval board, openSDA not working.

Jump to solution
3,164 Views
andrewparlane
Contributor IV

I have a FRDM-KL26Z eval board. I'm running the openSDA bootloader v1.11

From SDA_INFO.HTML:

Board Name is: FRDM-KL26Z

MicroBoot Kernel Version is: 1.05

Bootloader Version is: 1.11

Installed Application: PEMicro FRDM-KL26Z Mass Storage/Debug App

Application Version is: 1.14

I can boot into bootloader mode, and into the SDA application. The mass storage device appears. I see the expected contents.

However when I copy an srec from the precompiled examples in the quick start package from the FRDM-KL26Z freescale page (http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=FRDM-KL26Z&tid=vanFRDM-KL26Z) the openSDA led blinks a couple of times to indicate activity, and then goes solid. However nothing else happens. I've tried a few different applications, but no serial output / the RGB LED doesn't light up.

Opening laststat.txt before copying the binary says: "ready", after copying the binary and waiting 5s the file still says "ready". Power cycling the board has no effect either, other than the srec no longer is on the drive.

The demo app that came with the board worked fine, so it only stopped working after I reloaded the openSDA app as instructed in the quick start guide.

Anyone have any ideas?

Thanks

0 Kudos
Reply
1 Solution
2,545 Views
BlackNight
NXP Employee
NXP Employee

A common problem might be a virus scanner:

http://mcuoneclipse.com/2013/10/07/frdm-boards-not-responding-check-your-virus-scanner/

Or file manager/explorer extensions:

try to copy the file with the copy command from DOS Shell/command prompt.

View solution in original post

0 Kudos
Reply
3 Replies
2,546 Views
BlackNight
NXP Employee
NXP Employee

A common problem might be a virus scanner:

http://mcuoneclipse.com/2013/10/07/frdm-boards-not-responding-check-your-virus-scanner/

Or file manager/explorer extensions:

try to copy the file with the copy command from DOS Shell/command prompt.

0 Kudos
Reply
2,545 Views
andrewparlane
Contributor IV

Hi, that worked great, thank you.

I just tried using command prompt, and it worked straight off. I have terracopy (http://codesector.com/teracopy) as an alternative to windows copy, so that's probably the problem.

0 Kudos
Reply
2,545 Views
BlackNight
NXP Employee
NXP Employee

Yes, TeraCopy and other such 'accelerators' are source of problems for such bootloaders.

0 Kudos
Reply