FRDM-KL25Z compliance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-KL25Z compliance

1,262 Views
annaruggeri
Contributor I

Goodmorning,

I'd like to add the FRDM-KL25Z to a product I'm developing for the company where I work and industrialize it. I need understand if I can do it and if the development kit is compliant to IEC 60335 or similar.

Thanks a lot

Anna

0 Kudos
Reply
1 Reply

1,189 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Freescale provides IEC 60730 Class B library for Kinetis L series product.

More detailed info, please check below link:

IEC 60730 Safety Standard for Household Appli|Freescale

While, we don't have certification info about FRDM-KL25Z board hardware design if match with IEC 60335 standard.

Thank you for the attention.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply