FRDM-K66F samples

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-K66F samples

1,253 Views
a8Chcx
Contributor IV

Hi,

I am using FRDM-K66F180 and looking for demo application for SDRAM and Flexbus. But, I can't find in KSDK 2.0. Could you tell me where I can find these demo application?

Thanks,

Christie

Labels (1)
0 Kudos
Reply
1 Reply

1,069 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Christie,

     About the flexbus and the SDRAM demo application code, you can refer to the TWR-K65F180M KSDK2.0, you can download it from this link:

    https://mcuxpresso.nxp.com/en/welcome 

    Click build an sdk button, then select the TWR-K65F180M, and generate the code, you can find the flexbus and sdramc code in folder:

SDK_2.0_TWR-K65F180M\boards\twrk65f180m\driver_examples

Wish it helps you!
Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply