FRDM-K66F samples

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-K66F samples

1,252件の閲覧回数
a8Chcx
Contributor IV

Hi,

I am using FRDM-K66F180 and looking for demo application for SDRAM and Flexbus. But, I can't find in KSDK 2.0. Could you tell me where I can find these demo application?

Thanks,

Christie

ラベル(1)
0 件の賞賛
返信
1 返信

1,068件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Christie,

     About the flexbus and the SDRAM demo application code, you can refer to the TWR-K65F180M KSDK2.0, you can download it from this link:

    https://mcuxpresso.nxp.com/en/welcome 

    Click build an sdk button, then select the TWR-K65F180M, and generate the code, you can find the flexbus and sdramc code in folder:

SDK_2.0_TWR-K65F180M\boards\twrk65f180m\driver_examples

Wish it helps you!
Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信