FRDM K66F NOT WORKING AFTER UPDATING

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM K66F NOT WORKING AFTER UPDATING

1,349件の閲覧回数
Abhi3
Contributor I

My k66f frdm board doesn't wrk or get recognised on my pc anymore. I was working with it on MCU although i needed to work on a project in mbed studio therefroe i needed to update the board in order to make it work. I did the following steps and i used the following bin file to update my board.

https://www.nxp.com/downloads/en/snippets-boot-code-headers-monitors/k20dx_frdmk66f_if_crc_legacy_0x... 

The above link is the firmware's download link.

I followed the following steps:

1. Hold reset button then connect the USB to PC
2. A new volume called 'BOOTLOADER' should show up.
3. Copy the latest firmware into the disk, delete the .htm file if there is not enough space available.
4. The MCU should automatically load the new firmware and reconnect itself.
5. After reconnection, if the name of the volume changed (mine changed to FRDM-K66F, could be MAINTENANCE), the update should be successful.

At step 5, My volume didn't change name and instead it stopped working. Any help and suggestion will be appreciated.

ラベル(1)
0 件の賞賛
返信
1 返信

1,301件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, I understand the next you have the K66 EVK and want to change the firmware to the MBED studio. However, when you did this action the board changed to an unknown state. I recommend using the J-Link firmware to recover the board and then try the firmware for the MBED. 

OpenSDA Serial and Debug Adapter | NXP Semiconductors

About the MBED firmware is beyond the scope, do not have more information about that firmware.

Best regards,
Pavel

0 件の賞賛
返信