FRDM-K64F fail timeout

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-K64F fail timeout

1,603 Views
ricardo_zamorad
Contributor I

Compré una FRDM-K64F. Cuando la conecto a mi computadora, después de unos segundos se desconecta y vuelve a conectar y muestra un error de timeout. No me permite hacer nada porque se desconecta repetidamente.

0 Kudos
Reply
1 Reply

1,448 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Ricardo,

Please follow the next steps to update your FRDM-K64F firmware with JLINK. 

  1. Unplug the board, press the reset button and hold on it, then plug the cable to the board in J26, release the button. 
  2. You will find the board as a disc named "BOOTLOADER".
  3. Download the JLINK driver and install it. Link.
  4. Download the JLINK firmware for the FRDM-K64F. Link.
  5. Send the bin file to your board disc "BOOTLOADER". 
  6. Once it finished copying the file unplug the cable and plug it again. 

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 Kudos
Reply