FRDM-K64F BSP for FreeROTS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-K64F BSP for FreeROTS

1,677件の閲覧回数
cardoduplex
Contributor I

Has anyone a partial or complete Board Support Package for FreeRTOS. I have a maker project that I am developing with the FRDM-K64F. I have much of the RT tasks and inter-process communication completed, but development of BSP mapping is rather daunting.

0 件の賞賛
返信
1 返信

1,558件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Robert Blazewicz,

     About the FRDM-K64 BSP for FreeRTOS, you can refer to our K64 KSDK sample code which can be downloaded from this link:

Welcome to MCUXpresso | MCUXpresso Config Tools 

   Click SDK Builder, then choose the board as FRDM-K64, then generate the code and download SDK_2.2_FRDM-K64F.

pastedImage_2.png

pastedImage_3.png

After download, you can find the FRDM-K64 freeRTOS code in folder: \SDK_2.2_FRDM-K64F\boards\frdmk64f\rtos_examples

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信