FIT and reliability test report for the two components?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FIT and reliability test report for the two components?

1,793件の閲覧回数
tmao
Contributor I

Can I request you to share the FIT data and Reliability test report for the following two components: P82B96TD and 74LVC1G06GW. If possible can you also provide any other documents associated with the FIT and reliability such as the total number of samples tested so far, test duration and test temperature details? Finally, can I consider that Ea=0.7eV and CL (Confidence Level) = 60%

Thanks a lot !

0 件の賞賛
返信
2 返答(返信)

1,532件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Tony

For the P82B96TD you can find the FIT =2.0 on the following link:

Dual bidirectional bus buffer|NXP

For the 74LVC1G06GW FIT = 3.87

inverter with open-drain output|NXP

for more detail about the parameter for the test, please help me to create a new case on the following link:

Sales and Support|NXP

under

Regards

Vicente Gomez

1,532件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

vicentegomez​ can you help  to  review this case?

0 件の賞賛
返信