Example KV44F256 for usage of eFlexPWM with 312ps resolution

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example KV44F256 for usage of eFlexPWM with 312ps resolution

3,023 Views
katha
Contributor II

Hello,

I am looking for example code to use the eFlexPWM with 312ps resolution  within a KV44F256. Examples I found in SDK only provide setting the dutycyle 0...100%.

Thanks and regards

Labels (1)
4 Replies

2,663 Views
katha
Contributor II

Hi XiangJun,

that is what my question was for: could you send me the clocks configuration within a *.mex file?

Thank you and regards

Katharina

2,663 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Katharina,

Pls refer to the documentation, which describes the nano-edge placement feature of the KV46.

https://community.nxp.com/docs/DOC-341621

Hope it can help you

BR

XiangJun Rong

2,663 Views
katha
Contributor II

Hi XiangJun,

could you please send the .mex file including the clocks configuration

Thanks

Katharina

2,663 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Katharina,

I think the project does not use *.mex file, regarding the clock configuration, the clock configuration tools is not used, the clock configuration code for example PLL is integrated in the code in the main.c

BR

XiangJun Rong