Error in services launch sequence

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error in services launch sequence

ソリューションへジャンプ
24,933件の閲覧回数
srihariprasad24
Contributor II

Hai,

I am facing this error while debugging any codes(sdk example and new projects). i m using FRDM-KE16z Eval board. mke16Z64VLF4 controller. Kindly help solving.

 

thanks,

Hari.

 

0 件の賞賛
返信
1 解決策
24,865件の閲覧回数
ErichStyger
Specialist I

I see. So you have a DapLink (CMSIS-DAP) on your board. You need to connect to it using the LinkServer debug connection (not the P&E or Segger one).

 

I hope this helps,

Erich

元の投稿で解決策を見る

11 返答(返信)
24,894件の閲覧回数
ErichStyger
Specialist I

Hi @srihariprasad24 ,

Does pressing the 'Refresh' button in your screenshot help? If not, then your P&E debug probe is not recognized. If you are using the FRDM board with an on-board P&E firmware: make sure you are connected to the board.

If you plugin in the board, it should show up in your device manager, potentially showing up as a device on your host. Can you show a screenshot or tell us about what you see? If using Windows 10 and if your board has an old bootloader, you need to update the bootloader, see https://mcuoneclipse.com/2014/11/01/illustrated-step-by-step-instructions-updating-the-freescale-fre... and https://mcuoneclipse.com/2018/04/10/recovering-opensda-boards-with-windows-10/

 

I hope this helps,

Erich

0 件の賞賛
返信
24,900件の閲覧回数
srihariprasad24
Contributor II

Hi, pressing Refresh did not help, I have attached some screenshots. 1st one is an another frdm board that is working good and 2nd one is the one with issue.

0 件の賞賛
返信
24,895件の閲覧回数
ErichStyger
Specialist I

Hi @srihariprasad24 ,

is that COM5 from your board with the issue? If yes, the board is recognized but not as an P&E one.

What firmware did you load onto the K20 (if any)?

Does it show up as drive on your host? If so, the drive would show some diagnostic data.

 

I hope this helps,

Erich

 

0 件の賞賛
返信
24,892件の閲覧回数
srihariprasad24
Contributor II

FYI:

Eval board: FRDM- KE16Z

IC: KE16Z64VLF4

Software: MCUxpresso IDE

is that COM5 from your board with the issue?   YES

I m loading the sdk demo examples.

No diagnostics are shown in the drive, screen shot attached

0 件の賞賛
返信
24,890件の閲覧回数
ErichStyger
Specialist I

can you upload/share the content of the two files on the drive?

 

Erich

0 件の賞賛
返信
24,883件の閲覧回数
srihariprasad24
Contributor II

Hi, here it is

0 件の賞賛
返信
24,866件の閲覧回数
ErichStyger
Specialist I

I see. So you have a DapLink (CMSIS-DAP) on your board. You need to connect to it using the LinkServer debug connection (not the P&E or Segger one).

 

I hope this helps,

Erich

24,882件の閲覧回数
srihariprasad24
Contributor II

Debugging completed.

 

Thanks,

Hari

24,923件の閲覧回数
srihariprasad24
Contributor II

Hi, cant able to find any port name or address, what may be the issue? Can anyone help solving?

0 件の賞賛
返信
24,923件の閲覧回数
srihariprasad24
Contributor II

error3.jpgerror3.jpg

0 件の賞賛
返信
24,937件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

What's your debugger firmware of the board? When you plug the board to PC, do your PC show something like 'FRDM-KE16Z'. If not, hold the reset and then power on, do you see the disk like 'bootloader' or 'maintenance' 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信