Error While Debugging with Kinetic TWR-K53N512

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error While Debugging with Kinetic TWR-K53N512

5,264件の閲覧回数
communitycommun
Contributor III

Hello

   while debugging the MED-BPM code in IAR it shows some time of errors
the error is attached below

タグ(2)
5 返答(返信)

5,077件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello,

please, can you also attach debug log files?

Please, did you follow all these steps?

http://cache.nxp.com/files/microcontrollers/doc/user_guide/MEDBPMQSG.pdf?fromsite=zh-Hans

Thank you for your feedback!

Best Regards

Iva

0 件の賞賛
返信

5,077件の閲覧回数
communitycommun
Contributor III

The Debug log files say's as below:

Tue May 24, 2016 09:27:57: Missing or malformed flash loader specification file: C:\Program Files\IAR Systems\Embedded Workbench 7.3\arm\config\flashloader\Freescale\FlashK60Xxxx.board

for the past few day's its working very fine,suddenly these type of error has started from yesterday after the system restart

0 件の賞賛
返信

5,077件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello,

please can you try this trick?

Which .board file is correct for FRDM-K20D50M?

Please let me know, if this helps you.

Best Regards,

Iva

5,077件の閲覧回数
communitycommun
Contributor III

Thanks Iva...

its working now...it was helpful ,before your post i have also got the information from another site too..

Thanks for the support

5,077件の閲覧回数
communitycommun
Contributor III

I am already following that steps which you listed in PDF....
This program was running successfully,it collapsed after system restart 

0 件の賞賛
返信