Errata e7914 found in K64

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Errata e7914 found in K64

1,731 Views
mjbcswitzerland
Specialist V

Hi All

The K22 (and some KL devices) have a (minor) problem with the PIT according to e7914. See the following for K22:

Why do I need a delay after PIT clock enable?

The same difficulty has also been encountered with the K64 as reported here (with full details): http://www.utasker.com/forum/index.php?topic=1879.0

It seems therefore appropriate to add e7914 to the 1N83J errata sheet.

Regards

Mark

Kinetis: µTasker Kinetis support

K64: µTasker Kinetis FRDM-K64F support / µTasker Kinetis TWR-K64F120M support

For the complete "out-of-the-box" Kinetis experience and faster time to market

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,386 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Mark,

Thanks for your bug reporting,

I'll transfer this issue to Doc team for validation ASAP.
Have a great day and thanks again.
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply