EEPROM emulation by using FLASH memory?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EEPROM emulation by using FLASH memory?

Jump to solution
6,274 Views
pengliang
Contributor III

Hi all,

Does anyone know how to use flash memory emulate EEPROM? if yes, could you provide sample code tutorial?

Thank you

0 Kudos
Reply
1 Solution
3,763 Views
apanecatl
Senior Contributor II

You can download our flash drivers for EEPROM emulation in Non Flex NVM memory for Kinetis and ColdFire devices:

TFS Flash Driver Software for Kinetis and ColdFire+ Microcontrollers

If you are looking for EEPROM emulation using Flex NVM memory check the following App Note:

http://cache.freescale.com/files/32bit/doc/app_note/AN4282.pdf

View solution in original post

0 Kudos
Reply
4 Replies
3,763 Views
apanecatl
Senior Contributor II

You can download our flash drivers for EEPROM emulation in Non Flex NVM memory for Kinetis and ColdFire devices:

TFS Flash Driver Software for Kinetis and ColdFire+ Microcontrollers

If you are looking for EEPROM emulation using Flex NVM memory check the following App Note:

http://cache.freescale.com/files/32bit/doc/app_note/AN4282.pdf

0 Kudos
Reply
3,763 Views
pengliang
Contributor III

Thank you for the information.

Does the driver support Kinetis L family? thank you

0 Kudos
Reply
3,763 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Yes, you can even find an example in the installation folder of the C90TFS driver.

(Installation path)\Standard Software Driver vBeta033\C90TFS\Demos\L2K

3,763 Views
apanecatl
Senior Contributor II

I'm not pretty sure however the flash routines should be identical, so most likely yes

0 Kudos
Reply