Driver stepper motor ,KEA or KV?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Driver stepper motor ,KEA or KV?

2,264 Views
kigerzhang
Contributor III

Now there is a  medical automatic  injector instrument  project need  a MCU to control a stepper motor .

The MC34932 is planed to be  as the driver .

The KVxx is dedicated for motor driver . But the KEA xx seems more reliable.

The KEA series   and  KVxx  series  which is the best choice?

0 Kudos
Reply
1 Reply

1,925 Views
miduo
NXP Employee
NXP Employee

Hi,

It is really depend on your application, the requirement of your stepper motor.

Kinetis V Series MCUs are based upon the ARM® Cortex®-M0+, Cortex-M4 and Cortex-M7 cores and are designed for a wide range of BLDC, PMSM and ACIM motor control and digital power conversion applications.

The Kinetis EA series is an entry point to the broad ARM ecosystem and features:

  • A low-power ARM Cortex-M0+ core and 8–128 KB of embedded flash
  • Excellent EMC/ESD, high temperature and low radiated emissions
  • Scalable, highly robust performance solution for cost-sensitive automotive applications.

Attached you will find a PPT on this topic maybe helpful to you.

0 Kudos
Reply