Does the Kinetis MKV42F256VLL MCU has PWM outputs?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the Kinetis MKV42F256VLL MCU has PWM outputs?

1,408 Views
pierre_garon
Contributor I

As shown below, the NXP web site indicates that the MKV42F256VLL MCU has up to 18 PWM channels.

pastedImage_1.png However, as shown below, the KV4x Reference Manual indicates that the MKV42F256VLL MCU has no PWM outputs.

pastedImage_2.png

Also the MCUXpresso configuration tool indicates that there are no PWM outputs for the MKV42F256Vll MCU.

Thank you.

Pierre 

Labels (1)
1 Reply

1,305 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Pierre,

Although the KV42 doesn't have Chapter 38 Pulse Width Modulator A (PWMA/eFlexPWM) module, but the Chapter 40 FlexTimer Module (FTM) can be used to output PWM waveform too.

PWMA eFlexPWM FTM.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply