Does K60 have factory MAC address?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does K60 have factory MAC address?

1,888 次查看
chenghuang
Contributor I

the bit ADDINS in ENET_TCR  register ,when set it to 0,the meaning is “The source MAC address is not modified by the MAC.”。

1) Here “The source MAC address”,  is it factory MAC address?

2) Is it the only global ?

3) Can i use it in ethernet?

标记 (3)
0 项奖励
回复
1 回复

1,461 次查看
mjbcswitzerland
Specialist V

Hi

There are no MAC addresses programmed in the Kinetis devices - see Reading MAC address TWR-k60N512

The address that you are referencing is simply the one that the Ethernet software writes to registers with PALR and PAUR (used for reception address matching).

ADDINS is used to force the Ethernet controller to automatically insert this value also into transmitted frames (Ethernet II source address), whereby the Ethernet software usually does this itself.

Regards

Mark

Kinetis: µTasker Kinetis support

K60: http://www.utasker.com/kinetis/TWR-K60N512.html  / http://www.utasker.com/kinetis/TWR-K60D100M.html / µTasker Kinetis TWR-K60F120M support

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 项奖励
回复