Difference between processor on KEA64-TRK board and Automotive rated controller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Difference between processor on KEA64-TRK board and Automotive rated controller

ソリューションへジャンプ
2,511件の閲覧回数
stevencornett
Contributor III

We have been developing code using a TRK_KEA64 board that includes a PKEAZN64MLH2.  The processor we selected and placed on our
board is a S9KEAZN64AMLH.

From our perusal of the Freescale datasheets the two should be equivalent processors, but for some reason our P&E Cyclone for ARM is not able to load the algorithm used on the TRK board into the other processor

Is there an electrical or structural difference between the two processors that would preclude our programming the later with the algorithm and equipment used to successfully program the former?  If not, what are the correct settings?

ラベル(2)
0 件の賞賛
返信
1 解決策
2,414件の閲覧回数
stevencornett
Contributor III

The answer I received is as follows:

Yes, they are should be same. Would you please help to tell me how many chips did you test? Thanks.

I swapped boards and found that the second programmed normally.  All settings for the TRK worked for that device.

Thanks.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,415件の閲覧回数
stevencornett
Contributor III

The answer I received is as follows:

Yes, they are should be same. Would you please help to tell me how many chips did you test? Thanks.

I swapped boards and found that the second programmed normally.  All settings for the TRK worked for that device.

Thanks.

0 件の賞賛
返信
2,415件の閲覧回数
david_diaz
NXP Employee
NXP Employee

Hello Steve,

Indeed, the only difference between these two devices is the Qualification status. The rest of the its features are the same.

Capture.JPG

Best Regards,

David

0 件の賞賛
返信