Demo Code for getting DAC up and running on MK22Fn1M0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Demo Code for getting DAC up and running on MK22Fn1M0

1,415 次查看
achuthanparaman
Contributor I

I have a costume made development board with MK22FN1m0VLH12 chip op it.

On this board  I would like to get the DAC to do some task, to do that I would like to know if there is any demo code available out there? that i can use as ref.

Currently I am playing around with the demo code provided through "Freescale_MQX_4_0" bundle here the example/demo dose not include DAC, e.g. using IAR.

Any guidence / help is apprichiated

Thx in advance

标签 (2)
标记 (3)
0 项奖励
回复
1 回复

1,274 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Achuthan,

I attach an example of DAC, but it is based on K40, you have to modify it.

Hope it can help you.

BR

Xiangjun Rong

0 项奖励
回复