Demo Code for getting DAC up and running on MK22Fn1M0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Demo Code for getting DAC up and running on MK22Fn1M0

1,377件の閲覧回数
achuthanparaman
Contributor I

I have a costume made development board with MK22FN1m0VLH12 chip op it.

On this board  I would like to get the DAC to do some task, to do that I would like to know if there is any demo code available out there? that i can use as ref.

Currently I am playing around with the demo code provided through "Freescale_MQX_4_0" bundle here the example/demo dose not include DAC, e.g. using IAR.

Any guidence / help is apprichiated

Thx in advance

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 返信

1,236件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Achuthan,

I attach an example of DAC, but it is based on K40, you have to modify it.

Hope it can help you.

BR

Xiangjun Rong

0 件の賞賛
返信