Debug interface recommendations for Kinetis and LPC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debug interface recommendations for Kinetis and LPC?

617 Views
somaikoha
Contributor I

I do most of my development on the Kinetis series, and potentially some LPC parts in the near future. I've got a drawer full of debug interfaces from P&E Micro, including a Cyclone ACP that I use most.

I sometimes find myself switching from the $600 Cyclone to the $20 LPC-Link2 because the Cyclone has so many weird problems with MCUXpresso. Honestly the LPC-Link2 does most of what I need, it's just a bit slow.

Should I be looking at Segger interfaces? Can someone recommend a reliable, reasonably fast interface that's well-supported in MCUXpresso (and hopefully CodeWarrior 11 as well) that doesn't cause crashes all of the time, or fail to halt a running target? Trace support would be nice.

Thanks!

0 Kudos
Reply
2 Replies

521 Views
somaikoha
Contributor I

I do most of my development on the Kinetis series, and potentially some LPC parts in the near future. I've got a drawer full of debug interfaces from P&E Micro, including a Cyclone ACP that I use most.

I sometimes find myself switching from the $600 Cyclone to the $20 LPC-Link2 because the Cyclone has so many weird problems with MCUXpresso. Honestly the LPC-Link2 does most of what I need, it's just a bit slow.

Should I be looking at Segger interfaces? Can someone recommend a reliable, reasonably fast interface that's well-supported in MCUXpresso (and hopefully CodeWarrior 11 as well) that doesn't cause crashes all of the time, or fail to halt a running target? Trace support would be nice.  https://100001.onl/  

Thanks!

 

I got this,...

0 Kudos
Reply

601 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @somaikoha ,

Thanks for your post. For MCUXpresso, the LPC-Link is actually a good option, it has excellent compatibility and is quite inexpensive. However, it doesn’t appear to be supported by CodeWarrior. For instance, CodeWarrior v11.1 only supports the debuggers listed below.

Eclipse IDE for Microcontrollerss | NXP Semiconductors

Celeste_Liu_0-1779104226527.pngCeleste_Liu_0-1779104226527.png

 

Given that, you might want to consider getting a Segger J-Link.

Hope it helps.

BR

Celeste

0 Kudos
Reply