DMA performance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DMA performance

1,808 Views
martindusek
Contributor V

Hi,

what performance (MB/s) should I expect, when transferring data from GPIO (8-bit width GPIO0 - GPO7) on edge event on another GPIO pin to RAM using DMA?

Is 12 MB/s reachable when system clock = 96 MHz? 

Labels (2)
0 Kudos
Reply
2 Replies

1,681 Views
kaiyuewang
Contributor I

Hello, I am just trying to do the same thing as you. And I use the SCTimer match mode to send DMA trigger (in Burst Mode). It seems to me that the max frequency in this mode is about 10 MHz. 

Did you realize the transmission with a greater frequency? If yes, how?

0 Kudos
Reply

1,681 Views
miduo
NXP Employee
NXP Employee

Hi,

Please let me know the part number you mentioned. Thanks.

0 Kudos
Reply