Creating External Flash Algorithm for CW10.2 and Kinetis

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Creating External Flash Algorithm for CW10.2 and Kinetis

1,603件の閲覧回数
Icenine
Contributor I

Hello!

 

I found a document (AN3859) which describes how to create external flash algorithm for CW10 and ColdFire. I need to create such algorithm for Kinetis (we are using external flash).

 

AN3859 says that

 

- I need the sources of the Flash Tool Kit (FTK). But within CW10.2 package there are only sources for Coldfire.

  Where can I find FTK sources for Kinetis CPUs?

 

- I need the specification how CW10 passes the flashing parameters to the flash algorithm. AN859 describes it for the ColdFire CPUs (on Coldfire CPUs CW10 passes a pointer to the parameters within the D7 register). How is that done on Kinetis CPUs?  

 

Best regards

Johann

0 件の賞賛
返信
1 返信

1,395件の閲覧回数
ERussell
Contributor IV

I need the sources for the Kinetis FTK as well! I'm assuming that the setup for the flexbus can be included as part of the flash algorithm.

 

 

Thanks

0 件の賞賛
返信