Counter clock source and accessing the FTM CnSC and CnV registers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Counter clock source and accessing the FTM CnSC and CnV registers

Jump to solution
3,286 Views
jure1
Contributor I

Hello,

I am a starter in ARM programming and I am using MKE04Z8VTG4 MCU.

I am a bit unsure if I understood the reference manual correctly. If I use fixed frequency clock for timer clock source the frequency will be about 37.5kHz?

Is there any way to determine the exact frequency if I use 20MHz external crystal?

Also how do I determine the exact system clock if I use an external 20MHz crystal?

Are there any advantages/disadvantages for either of the clock sources (except the higher frequency of course)? I will require 10kHz frequency so I think it does not matter which one I choose.

Another problem I am having is writing to CnSC and CnV registers (FTM2). I can't seem to be able to figure it out how to do it.

For other registers I use for example: FTM2 -> POL |= (1 << 5)

So how do I write to these two in the same (similar) way?

I am still having a bit of problems figuring a lot of stuff out so I appreciate all the help (everyone was a beginner once) :smileyhappy:.

With regards, Jure

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
2,998 Views
Rick_Li
NXP Employee
NXP Employee

Hi Jure Stojs,

Please download KEXX_DRIVERS_V1.2.1_DEVD, the driver library package, it also contains a lot of examples for Keil.

View solution in original post

0 Kudos
Reply
4 Replies
2,999 Views
Rick_Li
NXP Employee
NXP Employee

Hi Jure Stojs,

Please download KEXX_DRIVERS_V1.2.1_DEVD, the driver library package, it also contains a lot of examples for Keil.

0 Kudos
Reply
2,998 Views
jure1
Contributor I

Thank you for posting this, I got everything I needed (and a lot more).

I got the timer configured properly and now it works.

0 Kudos
Reply
2,998 Views
Rick_Li
NXP Employee
NXP Employee

Hi Jure Stojs,

If you want a 10kHz, then, you have to use an external crystal.

MKE04 provides an internal low range reference clock, but this clock frequency can be multiplied by FLL or PLL to a very high frequency such like 20MHz.

For coding issue, I would suggest referencing demos of FRDM-KE04Z which can be downloaded from the below link:

Freescale Freedom Development Platform for th|Freescale

the file name is FRDM-KE04_QSP.

I hope it helps!

2,998 Views
jure1
Contributor I

I got the frequency and timing figured out, an external 20MHz crystal will be used (the same as for the system clock).

Unfortunately I can not open the examples since I use Keil uVision5 and there is still the problem with CnV and CnSC registers.

Another question about the timer functionality.

When the value in CnV register reaches a predefined value (1562) it sets the output to high.

Will the timer still count until it reaches the value stored in MOD register?

If yes that means I can use the timer interrupt to clear the previously set pin?

For example: The timer counts to 100 and at 100 it sets a pin high and continues to count.

The value in the MOD register equals a time of 110 so when the timer counts to this value it sets the interrupt and resets.

In the ISR i then turn the pin low and disable the timer (I enable the timer in another ISR).

So the pin would be 100us low, then 10us high and then low again.

I hope I was clear of what I am trying to achieve and if this is even possible. I read the datasheet and nowhere was written that this could not work but I am still unsure if it is possible :smileyhappy:.

Thank you for helping.

0 Kudos
Reply