Connecting K60D100m to External flash using flex bus interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Connecting K60D100m to External flash using flex bus interface

1,426件の閲覧回数
venkataprasad
Contributor II

Hi,

We are working on K60 evalution board to connect to micron external flash (M29W128GL) , using flex bus configuration (16 bit address and 16 bit data) in multiplexed mode. We have taken care of AD0 pin which is used only for data and not for address.

We are following example code of flexbus given by freescale.

IDE : IAR embedded workbench

please let me know if we are missing anything from the initialization code.

Even we are using micron flash drivers for flash init and checking comapatability but not getting right values.

void TWRK60_flexbus_init(void)

{

/* Enable the FlexBus                                               */

/* Configure the FlexBus Registers for 8-bit port size              */

/*  with separate address and data using chip select 0              */

/* These configurations are specific to communicating with          */

/*  the MRAM used in this example                                   */

/* For K60 tower module - do not set byte lane shift so that data   */

/*  comes out on AD[31:24]                                          */

  //Set Base address

  FB_CSAR0 = (uint32)&MRAM_START_ADDRESS; //0x60000000

  FB_CSCR0  =   FB_CSCR_PS(1)      // 8-bit port - Changed to FB_CSCR_PS(2) // 16 bit port

              | FB_CSCR_AA_MASK    // auto-acknowledge

              | FB_CSCR_ASET(0x1)  // assert chip select on second clock edge after address is asserted

              | FB_CSCR_WS(0x2)    // 1 wait state - may need a wait state depending on the bus speed

              ;

FB_CSCR0  |= FB_CSCR_BLS_MASK ;            Do we need to do this for k60??

  FB_CSMR0  =   FB_CSMR_BAM(0x7)  //Set base address mask for 512K address space

              | FB_CSMR_V_MASK    //Enable cs signal

              ;

   //enable BE signals - note, not used in this example

  FB_CSPMCR = 0x02200000;

  //fb clock divider 3

  SIM_CLKDIV1 |= SIM_CLKDIV1_OUTDIV3(0x3); // tried changing this also

  // Set the GPIO ports clocks

SIM_SCGC5 = SIM_SCGC5_PORTA_MASK | SIM_SCGC5_PORTB_MASK | SIM_SCGC5_PORTC_MASK |

SIM_SCGC5_PORTD_MASK | SIM_SCGC5_PORTE_MASK;

  /* Configure the pins needed to FlexBus Function (Alt 5) */

  /* this example uses low drive strength settings         */

  //address

  PORTB_PCR11 = PORT_PCR_MUX(5);           //  fb_ad[18]

  PORTB_PCR16 = PORT_PCR_MUX(5);           //  fb_ad[17]

  PORTB_PCR17 = PORT_PCR_MUX(5);           //  fb_ad[16]

  PORTB_PCR18 = PORT_PCR_MUX(5);           //  fb_ad[15]

  PORTC_PCR0  = PORT_PCR_MUX(5);           //  fb_ad[14]

  PORTC_PCR1  = PORT_PCR_MUX(5);           //  fb_ad[13]

  PORTC_PCR2  = PORT_PCR_MUX(5);           //  fb_ad[12]

  PORTC_PCR4  = PORT_PCR_MUX(5);           //  fb_ad[11]

  PORTC_PCR5  = PORT_PCR_MUX(5);           //  fb_ad[10]

  PORTC_PCR6  = PORT_PCR_MUX(5);           //  fb_ad[9]

  PORTC_PCR7  = PORT_PCR_MUX(5);           //  fb_ad[8]

  PORTC_PCR8  = PORT_PCR_MUX(5);           //  fb_ad[7]

  PORTC_PCR9  = PORT_PCR_MUX(5);           //  fb_ad[6]

  PORTC_PCR10 = PORT_PCR_MUX(5);           //  fb_ad[5]

  PORTD_PCR2  = PORT_PCR_MUX(5);           //  fb_ad[4]

  PORTD_PCR3  = PORT_PCR_MUX(5);           //  fb_ad[3]

  PORTD_PCR4  = PORT_PCR_MUX(5);           //  fb_ad[2]

  PORTD_PCR5  = PORT_PCR_MUX(5);           //  fb_ad[1]

  PORTD_PCR6  = PORT_PCR_MUX(5);           //  fb_ad[0]

  //data

  PORTB_PCR20 = PORT_PCR_MUX(5);           //  fb_ad[31] used as d[7]

  PORTB_PCR21 = PORT_PCR_MUX(5);           //  fb_ad[30] used as d[6]

  PORTB_PCR22 = PORT_PCR_MUX(5);           //  fb_ad[29] used as d[5]

  PORTB_PCR23 = PORT_PCR_MUX(5);           //  fb_ad[28] used as d[4]

  PORTC_PCR12 = PORT_PCR_MUX(5);           //  fb_ad[27] used as d[3]

  PORTC_PCR13 = PORT_PCR_MUX(5);           //  fb_ad[26] used as d[2]

  PORTC_PCR14 = PORT_PCR_MUX(5);           //  fb_ad[25] used as d[1]

  PORTC_PCR15 = PORT_PCR_MUX(5);           //  fb_ad[24] used as d[0]

  //control signals

  PORTB_PCR19 = PORT_PCR_MUX(5);          // fb_oe_b

  PORTC_PCR11 = PORT_PCR_MUX(5);          // fb_rw_b

  PORTD_PCR1  = PORT_PCR_MUX(5);          // fb_cs0_b

  PORTD_PCR0  = PORT_PCR_MUX(5);          // fb_ale

}

0 件の賞賛
返信
1 返信

1,257件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

From attached code, the 16-bit data port seems using FB_AD[31:24] pins as data port, which should belongs to below connection:

Flexbus.png

Then the CSCRn[BLS] bit should be 0.

As this connection, the FB_AD[31:24] should be 16-bit data port's high byte; and FB_AD[23:16] should be the low byte of 16-bit data port.

If it is possible, if customer could post the Flexbus related schematics for the double check.

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信