Connect NAND Flash by FlexBus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Connect NAND Flash by FlexBus

1,707 Views
Austin
Contributor I

I use K61 and K70 in our products now. I want to use the K65 in our new projects since it offers higher Flash and SRAM. I noticed the new Kinetis' has no NAND Flash Controller. Is it possible to connect NAND Flash via FlexBus?

Labels (1)
Tags (3)
1 Reply

1,341 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Austin,

It's possible to connect the NAND Flash directly by using the Flexbus interface, however it's not very usual and simple.

The problem is the NAND flash is block oriented and need some software error corrections.So it means that system needs software driver which takes care about this.

But we don't have such standalone driver for this now.

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------