Config tool support fot MKV31F128

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Config tool support fot MKV31F128

2,012件の閲覧回数
javadmccain
Contributor I

Hello  It seems that config tools does not support MKV31F128 peripheral (unlike processor expert in KDS). Is there any plan to add peripheral configurations in config tools? If yes, when? What are risks of keep using KDS for my projects?

ラベル(1)
2 返答(返信)

1,848件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Javad Mccain,

I just checked the latest MCUXpresso Config Tools v4.1 seems still not support MKV31F128 peripheral.
MCUXpresso Config Tools v5 will support it, and it is expected to be released in mid-November.
Hope these two threads about MCUXpresso and Processor Expert of KDS helps:
Porting Processor Expert Projects to MCUXpresso IDE
MCUXpresso IDE: Installing Processor Expert into Eclipse Neon

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,848件の閲覧回数
martinbra
Contributor II

Hi Robin.

We are at MCUXpresso Config Tools v6.0, and there's still no suport to MKV31F128 peripherals, just to the MKV31F512 peripherals.

DO you have any update if the support will be added?

Thanks In advance,

Martin

0 件の賞賛
返信