Codewwario10 .1 SE -License problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewwario10 .1 SE -License problem

2,803 Views
droga
Contributor I

Hello everyone

Recently installed the codewarrior 10.1 SE. everytime I try to compile an application or use codewarrior he asked to indicate the place where it installed the license, which in this case is not because it is a special version.

I spoke with support, but nothing was said about how to solve the problem.

if someone can help me how to solve this thank´s.

Thanks

0 Kudos
Reply
2 Replies

2,376 Views
dominate606
Contributor I

Update:

 

I did not find the registry mentioned, but I added  the line

FLEXLM_BATCH= -add 1

 to the file {Install path}\CW MCU v10.1\eclipse\cwide-env. The Popup is gone!

 

Dominik

0 Kudos
Reply

2,376 Views
dominate606
Contributor I

Hi droga,

 

I had the same problem, the builder asks for a license every time it is invoked. You can just close the window (red x). Depending on the complexity of the code, this has to be done several times.

 

I read about a solution on towergeeks, but I could not find the mentioned registry key. Somewhere else I found that it would be fixed with some hotfix, can't remember where.

 

Hope it helps,

Dominik

0 Kudos
Reply