Character LCD Solution for all Kinetis Parts

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Character LCD Solution for all Kinetis Parts

526 Views
mjbcswitzerland
Specialist V

Hi All

There is occasionally the requirement to integrate a low cost and low power character LCD into products.

In the following video I have shown how it is possible to set up a solution for any Kinetis part (I use the KL82 as example) connected by GPIOs and using a PWM output to control the LCD's contract which can be simulated, taking about 10 minutes in all.

https://youtu.be/YJEzxSqVtss

Full 8 bit or 4-bit nibble modes can be used and the complete user's guide is at http://www.utasker.com/docs/uTasker/uTaskerLCD.PDF

1 x 8 up to 4 x 20 (line/characters) are configurable.

Regards

Mark

Tags (2)
0 Kudos
Reply
0 Replies