Can't connect to K02 with USB Multilink

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can't connect to K02 with USB Multilink

跳至解决方案
4,515 次查看
arnogir
Senior Contributor II

Hello

I already used the pemicro USB multilink with Kinetis K60 and K70 (On CodeWarior and KDS)

Now, I start a new project on a K02 with MCUXpresso.

But when I want start the debug, I get the following error (like if target not connected) Refer to the attached jpeg.

What I should check first? (Blue Led and Orange Led are well light on on the PE micro Multilink universal.

To resume, the IDE is new for me and the microcontroller is new for me. then It is not easy to determine if problem comes from the hardware or something into MCUXpresso..

Please find the hardware schematic.

Thank for your help.

0 项奖励
回复
1 解答
4,428 次查看
arnogir
Senior Contributor II

Hello

It is an MK02FN64VLH10.

But I just found the problem, it was a short-circuit between TDO and TCLK.

But just a question, we link the JTAG Reset to the pin of MCU 'JTAG-RST' wichi is by defaut a gpio pin function.

Then Should we instead link the Jtag reset to the RESET pin of the MCU K02?

在原帖中查看解决方案

0 项奖励
回复
7 回复数
4,428 次查看
arnogir
Senior Contributor II

Hi,

Following is that I use because it was I used in CW and KDS..

PEMicro.jpg

I don't now the 'LS' connection. How associate it to the Pemicro probe? It ask me a "LinkServer"??

-Then finally, what is the advantage of the SWD related to the JTAG?

-Is cyclone Fx has the SWD link? (used in production)

0 项奖励
回复
4,428 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Arnaud Girard,

  In fact, you are using the SWD interace in your code.

pastedImage_1.png

Your debugger can support the SWD.

Now, what's the debugger result?

Do you have Segger JLINK on your side? If yes, you can use the JLINK commander to connect your board at first, whether you can find the ARM core or not? If you can't find the ARM core, it means your hardware still have problems.

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
4,428 次查看
arnogir
Senior Contributor II

Hello,

I do not know this interface.

Is it is present on USB Multilink universal PortF used for Kinetis?

What is the difference on the using? On the MCUXpresso debugging interface?

How configure MCUXpresso to switch from the JTAG to SWD?

0 项奖励
回复
4,428 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Arnaud Girard,

   Multilink can support the SWD directly.

pastedImage_1.png

Other port is the same, you just need to use the SWD_DIO, SWD_CLK, RESET, VCC and GND.

Kinetis chip related pin: PTA3 is SWD_DIO, PTA0 is SWD_CLK. RESET is your MCU RESETB.

About the MCUXPresso IDE, do you modify the JTAG debugger interface? If not, it should in default using the SWD.

pastedImage_1.png

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
4,428 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Arnaud Girard ,

 

    Please tell me your K02 chip full name, the part number, your schematic picture partnumber name also is not completed.

   Please give me you chip partnumber, then I can help you to check more details.

Waiting for your updated information.

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
4,429 次查看
arnogir
Senior Contributor II

Hello

It is an MK02FN64VLH10.

But I just found the problem, it was a short-circuit between TDO and TCLK.

But just a question, we link the JTAG Reset to the pin of MCU 'JTAG-RST' wichi is by defaut a gpio pin function.

Then Should we instead link the Jtag reset to the RESET pin of the MCU K02?

0 项奖励
回复
4,428 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Arnaud Girard,

   Thanks for your updated information.

   Do you try the SWD interface instead of JTAG?

  SWD_DIO is better to add external 10K pull up.

   Reset_b pin need to add external 10K pull up and 0.1uf capacitor to ground.

  About the reset,  normally, we connect the MCU reset_b pin to the SWD interface.

  It means, the SWD interface have these signals: SWD_DIO, SWD_CLK, RESET_b, VDD and GND.

  Can you accept the SWD interface?

   

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复