Hi Kostas Nomikos
Yes, it is possible. Are you using KL43 or KL46? These two devices have different clock module (MCG and MCG-lite). I recommend you the following link:
https://www.nxp.com/files-static/training_pdf/28973_S08_MCG_WBT.pdf
It is for MCG and it explains in detail the different clock modes. Actually, out of reset, Kinetis devices work in FEI mode which doesn't run to the 48MHz.
I highly recommend you SDK software tools, You can download it from
https://mcuxpresso.nxp.com
It includes a clock config tool where you can set the frequency that needs.
Hope this information could help you, please don't hesitate to contact me if you have any other question about this.
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------