Can USB-KW24D512 USB work with the internal crystal (FEI mode)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can USB-KW24D512 USB work with the internal crystal (FEI mode)?

1,789 Views
luwan
Contributor II

I am trying to enable USB on USB-KW24D512. Is the USB able to work with the internal clock (working at FEI mode)?

0 Kudos
Reply
3 Replies

1,648 Views
miduo
NXP Employee
NXP Employee

Hi,

We really do not recommend to using the FLL to clock the USB module, that will led a non-working USB applications. The MCGFLLCLK does not meet the USB jitter specifications for certification.

pastedImage_1.png

0 Kudos
Reply

1,648 Views
luwan
Contributor II

Hi,

I am now using PLL (PEE mode) and the USB CDC is able to shown as ACM0 (enumeration successfully).

But the board fails to tx/rx traffic, are there any guide lines to help for troubleshooting?

0 Kudos
Reply

1,648 Views
miduo
NXP Employee
NXP Employee

Hi,

Please let me know the what board you are using? The customer board or the evaluation board?

0 Kudos
Reply