Can I use FRDM-K22F eval board with MK22FN512VLH12 MCU on it to run code built for MK22FN256CAH12 MCU

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can I use FRDM-K22F eval board with MK22FN512VLH12 MCU on it to run code built for MK22FN256CAH12 MCU

866 次查看
priya_dwivedula
Contributor III

Can I use FRDM-K22F eval board with MK22FN512VLH12 MCU on it to run code built for MK22FN256CAH12 MCU? I am able to flash the code the eval board but it's getting struck up in startup.c.

标记 (1)
0 项奖励
回复
1 回复

795 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

With the default (P&E) firmware on the FRDM-K22 it is not possible to debug another processor, except the device on the FRDM board itself.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复