Can FlexBus be connected to SRAM like this?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can FlexBus be connected to SRAM like this?

2,639件の閲覧回数
ljjtczr
Contributor I

Hi

FlexBus's FB_AD1~FB_AD18, which should  been connected to SRAM's A0~A17 .

The PCB board has been completed, and then we need to replace the SRAM . The new SRAM's address line is one pin less than the old. It has changed a NC pin in the middle of the address line.

So FB_AD1~FB_AD5 is connected to A0~A4, FB_AD6 is connected to NC useless, FB_AD7~FB_AD18 is connected to A5~A16. I want to ask, can it be used normally?

Thanks

タグ(1)
0 件の賞賛
返信
4 返答(返信)

2,434件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

What part number you mentioned?

0 件の賞賛
返信

2,434件の閲覧回数
ljjtczr
Contributor I

before:

pastedImage_5.png

now:

pastedImage_4.png

0 件の賞賛
返信

2,434件の閲覧回数
miduo
NXP Employee
NXP Employee

I mean the Kinetis part you connected with this SRAM.Thanks.

0 件の賞賛
返信

2,434件の閲覧回数
ljjtczr
Contributor I

MK64FN1M0VLQ12

0 件の賞賛
返信