CDC enumeration not happening in KL25 microcontroller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CDC enumeration not happening in KL25 microcontroller

2,840件の閲覧回数
deepaksingh
Contributor II

Hi, i am using kl25 series and i have configured FSL_USB_STACK for both USB_OTG and CDC. Using this configuration I have compiled and flashed into kl25 board. But after connecting USB to the device, device is not showing inside device manager.we refered below link http://mcuoneclipse.com/2012/10/07/tutorial-usb-cdc-with-the-kl25z-freedom-board/.

ラベル(2)
0 件の賞賛
返信
6 返答(返信)

2,676件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Deepak,

are you using Kinetis Design Studio V2.0.0?

Erich

0 件の賞賛
返信

2,676件の閲覧回数
deepaksingh
Contributor II
0 件の賞賛
返信

2,676件の閲覧回数
yasuhikokoumoto
Senior Contributor I

Hello Erich,

did you connect J21 jumper on the board?

If you already did it, I'm sorry.

Best regards.

Yasuhiko Koumoto.

0 件の賞賛
返信

2,676件の閲覧回数
BlackNight
NXP Employee
NXP Employee

there is no J21 jumper on the FRDM-KL25Z, or did I miss it?

I'm using the board with its default jumper settings/configurations.

0 件の賞賛
返信

2,676件の閲覧回数
yasuhikokoumoto
Senior Contributor I

Hello Erich,

really?

I am afraid the board had been revised.

Does your board have the below jumper?

Because no header for J21 is equipped and you should attach the header.

pastedImage_3.png

Best regards,

Yasuhiko Koumoto.

0 件の賞賛
返信

2,676件の閲覧回数
BlackNight
NXP Employee
NXP Employee

oh, I missed that jumper, sorry. So I do have this jumper *not* set.

0 件の賞賛
返信