BLE Connection Interval Events

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BLE Connection Interval Events

2,024 Views
ibrahimyoussef
Contributor I

Hello!

I am working on a project with three NXP FRDM-KW41Z boards, and I have them communicating data via Bluetooth Low Energy. One board is being used to collect the data sent by two peripheral devices, which send notifications periodically. I am looking to synchronize the data collection to the connection interval, and was wondering how/if this could be done. I am unable to find anything like a callback function that is called at the start/end of a connection interval, but was hoping that there is some other way to "listen" for the start of a new connection interval on the peripheral devices.

In a nutshell, is there any event or callback function on the peripheral devices that I could exploit to indicate that a connection interval has just begun?

Thanks in advance!

Best,
Ibrahim

0 Kudos
Reply
1 Reply

1,661 Views
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

Unfortunately, we do not have a function or guide to identify what you are looking for.... sorry for the inconvenience this might cause you. 

Best regards, 

Estephania 

0 Kudos
Reply