BGA package running hotter than LQFP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BGA package running hotter than LQFP

ソリューションへジャンプ
2,563件の閲覧回数
odd_bikes
Contributor III

Hi,

Because of the chip shortage we've recently switched our products from the 144LQFP package to the 121XBGA (MK66FN2M0VLQ18 to MK24FN1M0VDC12). We've noticed that, with the BGA package, the MCU currently sits at about 50-60* C package temperature while drawing the same amount of current as the previous one we've used. It's significantly hotter than the LQFT version we've used before.

Is this normal? Obviously, being a smaller package and the same thermal energy being dissipated, that could be an explanation, but we'd obviously like to check first.

Regards.

Alex

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 解決策
2,401件の閲覧回数
odd_bikes
Contributor III

Just as an update. We had indeed a schematic problem, whereby 5V were being put through the supply pins for the ADC. As soon as that was corrected, there were no more thermal issues.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,544件の閲覧回数
PabloAvalos
NXP TechSupport
NXP TechSupport

Hi @odd_bikes

 

Hoping you are doing well.

 

Effectively, as the 121XBGA is smaller than 144LQFP package, the same thermal energy to be dissipated in a smaller area is higher.

 

Please let me know if you have more questions.

 

Sincerely,

Pablo Avalos.

2,402件の閲覧回数
odd_bikes
Contributor III

Just as an update. We had indeed a schematic problem, whereby 5V were being put through the supply pins for the ADC. As soon as that was corrected, there were no more thermal issues.

0 件の賞賛
返信