Available pins for TRACE_CLKOUT on K64

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Available pins for TRACE_CLKOUT on K64

Jump to solution
1,921 Views
aberger
Contributor V

I am using a K64F in MAPBGA 144 package and have a debug header wired to the MCU requiring routing of the TRACE_CLKOUT signal to pin D3. The K64 Sub-Family Data Sheet indicates in the Pinout chapter that pin D3 can be routed for TRACE_CLKOUT using the ALT5 mux configuration. By contrast, I noticed that in the MCUXpresso Config Tools > Pins view > Peripheral Signals tab, the SIM > CLKOUT signal only has two pins available to it: A11 and J7. This is in direct conflict with the K64 Sub-Family Data Sheet. Which information is accurate?

Labels (1)
0 Kudos
Reply
1 Solution
1,856 Views
nxf56274
NXP Employee
NXP Employee

Hi,

The D3 is not belong to the SIM. It belongs to TPIU. You will find D3 under the peripheral TPIU.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

1 Reply
1,857 Views
nxf56274
NXP Employee
NXP Employee

Hi,

The D3 is not belong to the SIM. It belongs to TPIU. You will find D3 under the peripheral TPIU.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------